This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62005: 芯片默认配置下,U3、U4有正确输出,U0、U1、U2无输出时钟波形

Part Number: CDCE62005

我注意到芯片的默认工作情况为下图所示:

我现在使用AUX_IN输入25MHz单端时钟(方波  2Vpp  无偏置  HiZ)

此时PLL_LOCK为持续高电平——PLL成功锁定,且U3和U4有正确频率的波形,但U0、U1、U2只有直流偏置却没有输出时钟波形,请问这可能是什么原因呢?

另外,U3和U4的输出偏置电压为1.6V,正常吗?我使用的输入时钟应不应该设置偏置?

【补充说明:】

实测整个芯片的各个VCC引脚均供电正常,VBB为1.38V也正常,外部配置引脚REF_SEL、PowerDown、SYNC均为高电平。

期待您的指点和回复!谢谢!

  • AUX_IN 是LVCMOS输入,VCC=3.3V的话,Vih(min)=0.7*Vcc. 所以输入2Vpp方波不满足幅值范围,建议输入0~3.3V。

    另外,U3默认输出LVDS电平,LVDS偏置电压是1.24V,幅值范围位270mV~550mV。

    U4默认输出为LVCMOS。所以不应该是1.6V偏置,输出Voh和Vol如下: