This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594EVM: 信号锁定时间长。时钟超过5M,无法控制芯片。

Part Number: LMX2594EVM

  1. spi信号时钟为1M,可以顺利控制芯片生成频率。时钟为5M,控制失效,时钟远低于手册给的50M限制。通过示波器观察,时钟在1M和5M,信号差别仅在于5M时钟的信号,其上升延后的震荡更大,上下浮动电平差,不超过0.8V。
  2. 2594的锁定时间通过频谱观察信号,锁定时间在1.6ms的量级。远高于手册us级的锁定时间。
  3. 请问如果要缩短锁定时间,应该怎么操作