This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2492: 工作一段时间后微波失锁,并且内部寄存器恢复成上电值。

Part Number: LMX2492


您好,我们最近使用LMX2492过程中发现一个问题,我们查找了一段时间没找到故障原因,特向大家求教。

目的:

        LMX2492产生一个3.4GHz的频率。

故障现象:

       产品在测试过程中发现3.4GHz输出失锁定。故障复现时间没有明显规律,有时候四五个小时都能一直正常锁定,有时候连续输出失锁(几分钟就失锁)。

故障排查过程:

       1.不确定失锁原因情况下,我们重新配置寄存器使MUXout输出R Divide/2频率(频率等于5MHz)等待故障复现。故障发生后我们发现3.4GHz失锁并且MUXout管脚上5MHz输出消失(LMX2492无硬件复位管脚,只有软件指令复位)。

        2.根据上述情况我们又加入LMX2492内部寄存器读取功能,先读取正常工作时LMX2492内部寄存器值 ,然后等待故障复现。故障复现后我们又读取了LMX2492内部寄存器的值。再读取了上电复位后不进行初始化配置的LMX2492内部寄存器值。对比上述三组寄存器值发现:LMX2492脱锁后的内部寄存器值和LMX2492上电复位后内部寄存器值一致。得出结论:LMX2492内部寄存器值产生了变化导致微波失锁,MUXout输出消失。

       3.根据上两条,我们怀疑电源波动、或者共用SPI总线导致误操作写入导致LMX寄存器值被改写。我们使用示波器观察LMX2492 LE管脚在故障发生前后均无波动,并且LMX2492和单片机共用电源,故障过程后单片机状态正常无复位发生。

我们在分析很久后没有找到故障原因特向大家请教。