Part Number: LMH1981
Other Parts Discussed in Thread: LMH1982, , LMK1C1102, LMH1228
LMH1981+LMH1982作为genlock器件,搭配哪科芯片可以实现ref IN,同时环出ref IN
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您的意思是从LMH1981 的REF IN进入,然后回环再从REFIN输出是吗?
可是LMH1981+LMH1982搭配,这两颗芯片内部都没有回环通路呢?或者您把您的应用框图附上以便理解。
明白了,所以您这里需要的器件有两个功能,一个是buffer,一个是扇出。
所以我选了一款LMK1C110x系列的buffer,这个系列一共可以 1:2, 1:3, 1:4三种输出,LMK1C1102可以满足您的需求,一路输入,两路输出同样的信号输出,然后一路给其他设备,一路进入LMH1981. REFIN是单路LVCMOS电平吗?您可以参考下这款buffer的数据手册,看下电气参数是否满足 您的要求
https://www.ti.com/lit/ds/symlink/lmk1c1102.pdf

那可以试试LMH1228这课redriver,带自环模块,如下架构图。可以应用于HDTV或SDTV 视频应用,我看它的幅值范围是满足LMH1981输入幅值要求的,LMH1981输入幅值典型值300mV(SDTV)和600mV(HDTV)。符合1228的输入要求。可以实际验证下。



另外补充下,就是可能1228在您的应用中有点儿浪费,您应该不需要对信号进行补偿,从REFIN换回出来也不会经过长的cable传输,所以1228实际是一款redriver/reclock,主要是对信号在长距离传输过程中发生的衰减,随机产生的抖动进行补偿。所以需要您这边实际验证下,如果不可行的话,就没有其他器件推荐了。