Part Number: LMX2592
你好,LMX2592如果将 OUTA_PD = 1;OUTB_PD = 1;为什么芯片还是很烫,正常使用情况下温度大概有多少,对于温度的变化可以提供一下参考吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2592
你好,LMX2592如果将 OUTA_PD = 1;OUTB_PD = 1;为什么芯片还是很烫,正常使用情况下温度大概有多少,对于温度的变化可以提供一下参考吗
您好,LMX2592的结温不超过125度就就可以。这颗芯片的热阻很高,thetajA=30.5C /W, 也就是说每上升1W的功率,温度上升30度。
所以这颗器件有thermal pad,您是否已经将thermal pad铺铜接GND,来提高它的散热?
另外,您有测试它的供电电流吗?OUTA_PD = 1;OUTB_PD = 1条件下,理论上供电电流在3.7mA左右,您测试下看看是否超过这个值?
你好,那我如果停止它就必须关闭他的电源才行吗,我是用测温仪测量了一下他的温度发现有五六十左右
那我如果停止它就必须关闭他的电源才行吗
低功耗状态下,就像您上述,将OUTA_PD = 1;OUTB_PD = 1使其处于power down状态下即可。
根据手册在OUTA_PD = 1;OUTB_PD = 1 下VCC供电电流为3.7mA左右,此时功耗3.7mA*3.3V =12.21mW。可以计算下理论上结温:
Tj=12.21mW *30.5C /W+25C =25.37C左右。所以如果您 测试得到5,6十度的样子,和数据手册是不符的。功耗相对来是说有点儿大。