Part Number: LMK5B12204
Other Parts Discussed in Thread: LMK05318B
您好,TI
我用TICS Pro软件设置XO频率为10MHZ,设置OUT2端口为CMOS(+/-),Target freq(HZ)为100MHZ,并关闭了Enable PRIREF和Enable PRIREF,使用I2C+EEPROM配置了LMK5B12204的寄存器,配置成功了,但是OUT2端口用keysight 53230A测试实际频率只有 99.5MHZ左右的频率,跟100MHZ相差太大,为什么会出现这样精度相差太大的情况,难道是不该选用10MHZ的XO吗,此频点不对?如果此频点不对的话,选用的XO的频率应该符合怎样的标准。另外,PRIREF freq(HZ)和SECREF freq(HZ)的输入频率有何要求,是否可以使用10MHZ的OCXO。因为我司想用10MHZ的OCXO的晶振来产生频率,市面上大多的OCXO也是10MHZ,很少有12.8MHZ、48.0048MHZ的OCXO,所以来咨询这个问题。另外如果这款时钟芯片不能采用10MHZ的OCXO来产生高精度,低抖动频率,是否有贵公司的别的时钟芯片来代替?如果有的话请提供一下