This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2592: 相关功能请教

Part Number: LMX2592


刚接触lmx2592,想请教一下一些2592功能的问题:

1、上电后不设置参数的情况下能直接读取PLL的输出频率吗?

2、A,B两路的输出频率可以单独设置吗,使两路输出不一样输出频率?两路的输出功率我看是可以单独设置的OUTA_POW和OUTB_POW

  • 您好

    1、

    您想读取输出频率需要上述参数,但是在上电后这些参数有默认值

    但是这些些默认值没有相关使能,根据datasheet显示应该不能直接读取。

    2、

    请看上图显示关于OUTA_POW和OUTB_POW取决于输出增益可以分别设置,而频率如上图和表都是需要多个寄存器进行统一配置的。请您参考。