This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4024芯片工作电压为5V时,时钟输入频率最大为多少MHZ?



In the table below the RECOMMENDED OPERATING CONDITIONS in the CD4024 chip specification, when the chip is operating at 5V, the maximum input pulse frequency is 3.5MHZ; In the table below DYNAMIC ELECTRICAL CHARACTERISTICS, when operating at 5V, the maximum pulse input range is 3.5-7MHZ; What is the difference between these two, and which of the actual working maximum frequency should prevail?