Part Number: LMC555
我现在画的一块有LMC555芯片构成的单稳态触发电路,传播延时为80ns,请问我有什么办法能将其调到10ns以内


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
关于LMC555器件的传播延时,其最小可以达到的具体数值并不是一个固定的值,因为它受到多种因素的影响,包括电路设计、工作条件以及器件本身的制造工艺等。
官方datasheet给出以下参数参考。

(1)减少寄生参数:
(2)选择高速元件:
尽管调整电阻和电容值对于减少纳秒级的延时作用有限,但在某些情况下仍然值得一试。然而,需要注意的是,过小的电阻和电容值可能会导致电路不稳定或无法正常工作。
总结
将LMC555芯片构成的单稳态触发电路的传播延时从80ns调整到10ns以内是一项困难的任务,因为这涉及到芯片内部的物理限制和电路设计的复杂性。可能需要重新考虑电路设计、选择更快的元件或采用其他技术来实现所需的延时功能。在任何情况下,都建议进行充分的测试和验证以确保电路的稳定性和可靠性。