This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVP1102: 正弦波驱动CDCLVP1102

Part Number: CDCLVP1102


您好!

请问cdclvp1102可以接受正弦波输入,然后转换为两路LVPECL输出吗?

谢谢!

  • 您好

    关于CDCLVP1102是否可以直接接受正弦波输入,我们需要考虑以下几点:

    • 输入电平要求:正弦波作为一种波形,其电压和电流随时间连续变化。而CDCLVP1102的输入端是设计来接受特定电平(如LVPECL、LVDS、LVCMOS/LVTTL)的数字信号。这些信号具有明确的逻辑高和逻辑低电平。
    • 信号转换:正弦波信号需要被转换为适合CDCLVP1102输入的电平信号。这通常需要使用某种形式的信号调理电路,如比较器或模数转换器(ADC),将正弦波转换为数字信号。

    CDCLVP1102本身不接受正弦波输入。它设计用于处理数字电平信号,如LVPECL、LVDS、LVCMOS/LVTTL等。如果需要将正弦波输入转换为LVPECL输出,需要先使用适当的电路将正弦波转换为CDCLVP1102可接受的数字电平信号,然后再利用CDCLVP1102进行缓冲和分发。