This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL5010: TPL5010

Part Number: TPL5010

你好有个问题想请教一下,我们公司现在使用的TPL5010DDCR,配置的169K电阻,想要两小时复位一次,但是发现有四小时复位一次的现象,是什么原因导致的呢.?我很好奇?

  • 感谢您对TI产品的关注!
    关于你的咨询,你用的Rext太小了吧,超出推荐范围了。

    可能是因为超出范围不稳定。

  • 你好,非常感谢你能回复我的问题,我的Rext使用的是169K,单位是kΩ不是169Ω,精度为1%。
    2、好像也有复位失效的问题,重新上电后一直没有打印信息,是不是复位失效了
    3、在计时周期内发送第二个DONE信号的时候,是否会刷新计时周期?比方说我现在计时周期为2小时,我在30分钟的时候发送第一次DONE信号,然后我在1个小时的时候发送第二次DONE信号,这时候是否会刷新计时周期二小时

  • 那你换个芯片看看,可能跟这个芯片关系不大,这芯片外围也没什么电路。