This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK3H0102: TICS PRO中的PCIE Refence Clock analysis tool,生成PCIE时钟report失败?

Part Number: LMK3H0102


把PNA测试的LMK3H0102产生的100M时钟的测试数据(.csv) 导入到TICS PRO中的PCIE Refence Clock analysis tool中,但是生成报告失败,请问如何解决?

CSV文件格式如下:

Center Frequency [Hz]
99752047.11
Frequency [Hz] Phase Noise [dBc/Hz] Phase Noise - no spurs [dBc/Hz]
1000 -15.632934 -112.100189
1000.345398 -15.645643 -112.103188
1000.690857 -15.65835 -112.106194
1001.036987 -15.80165 -112.109192
1001.382751 -15.957776 -112.11219
1001.728577 -16.113876 -112.115189
1002.074524 -16.304064 -112.118195
1002.420654 -16.606348 -112.121193
1002.767395 -16.909061 -112.124191