Part Number: TPL5010
DELAY管脚下拉使用47K,按照参考手册应该是6min不喂狗被唤醒,但实际时间为10min左右。
下拉使用30K,理论应该是2min,实际是4min
也尝试在4管脚DONE下拉10K电阻到GND,但没有效果


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
下面哪个时间间隔不正确?是WAKE信号还是RSTn到WAKE时间间隔?

tip 是 6 mins or 360s or 360000ms.
如果 T2 是 100ms, 那么 t = 360000ms - 100ms + 360000ms = 719900ms = 11.998333 mins.