Part Number: LMK05318BEVM
Other Parts Discussed in Thread: LMK05318B, LMK5B33216
我以GPS模块输出的1pps信号作为评估板的PRIREF输入,同时配置使用了12Mhz的TCXO。我用OUT7输出了1hz时钟信号,但OUT0-OUT6均无法成功生成我需要的4Khz时钟信号。请问这种情况如何解决呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK05318BEVM
Other Parts Discussed in Thread: LMK05318B, LMK5B33216
我以GPS模块输出的1pps信号作为评估板的PRIREF输入,同时配置使用了12Mhz的TCXO。我用OUT7输出了1hz时钟信号,但OUT0-OUT6均无法成功生成我需要的4Khz时钟信号。请问这种情况如何解决呢?
LMK05318B不支持OUT0至OUT6的输出频率低于3.0692 MHz。
只有OUT7可以输出低频(如4 kHz或1 Hz),因为它包含两个分频器以获得较小的频率。
较新的部件LMK5B33216可以通过SYSREF输出通道支持4 kHz输出(有12个SYSREF通道可用于输出4 kHz)。