This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2572: 没有参考信号时,配置频率字,芯片会出现“死机“的情况,必须采用reset复位才能恢复正常

Part Number: LMX2572

我们在用LMX2572时,出现一个很奇怪的现象,LMX2572在上电后,使用spi成功锁定一个频率,然后把参考信号(Oscin)断开,再配另一个频率字,写入一次R0寄存器,寄存器操作结束以后,再把参考信号(Oscin)加上,此时会随机出现两种现象:

1、一种是锁相环失锁,但重新配一次频率字以后,能够恢复锁定,后面继续跳频也都能工作正常;

2、另一种是芯片的电流比正常工作时,电流大了30mA,失锁,并且从这以后不管怎么操作频率字,都没有办法恢复锁定了,这个时候,必须要采用R0寄存器中的Reset位复位,芯片才能恢复正常工作;

我想问一下,为什么会出现两种不同的现象,这两种现象出现的机理是什么?