This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04610: USB2ANY控制LMK04610

Part Number: LMK04610
Other Parts Discussed in Thread: USB2ANY, ,

我的电路完全参考LMK04610EVM的原理图设计,开始USB2ANY与电路板连接没有任何问题,也可以正确的控制LMK04610。现在将USB2ANY与电路板连接后,供电电流明显增加,类似短路的现象。经过排查,将图中红叉处断开,就恢复正常了。这可能是什么原因呢,USB2ANY没配置对?

  • 已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 您好

    根据我的研究,似乎U10针5选择方向。
    有效地,U2A_STAT1将通过A1输出。
    我不认为USB2ANY配置不正确。
    在EVM用户指南上,也没有填充R232。


    在EVM用户指南中,它可用于回读或锁定检测,具体取决于EVM上的开关位置。
    但在许多情况下,U2A_STAT1可能会被拉动,最终可能会消耗一些电流。