Part Number: LMK03318
我们将时钟参数写到EEPROM中,上电后LMK03318 STATUS0/STATUS1管脚状态是输出为1/0,此时我们系统需要时钟的器件A工作正常。然而多次上下电后,需要时钟的器件A工作不正常的问题,此时LMK03318 STATUS0/STATUS1管脚输出为0/0,重新上下电后又能恢复正常。
R13配置值为0x00、R27配置值为0x20、R28配置值为0x10,出现异常后R13读出来的值为0x80
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
R137.6 REGCOMMIT位是在转换完成后自动恢复为0,在“10.5.4 Write SRAM”中有此功能的写入流程请检查。
您好,
而且我们的程序操作了几十片芯片,只有2片遇到了“R137.6一直没有自动恢复为0”的情况
请问检查了出问题的2片EEPROM有正确编程成功吗?电路间是否有差异,是否做了交叉测试?