Other Parts Discussed in Thread: DS90C365A, TVP7002, DS90C363B
您好!我现在有一个项目,输出的是R , G, B, HS,VS,信号。但是液晶显示屏是LVDS(3data+1clock)的接口。我想问选用什么芯片能够将这个5个脚的输出与液晶屏无缝连接。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好。我看了TVP7002的手册。我想知道的是该芯片能否将输入的模拟信号转换为6bit的数据输出。我不需要8bit的数据。是否我舍掉低两位就可以实现呢?还是需要设置。谢谢!
你的意思是输出RGB666,可以的,采用高6位,对于TVP7002来说,不用的输入端通过10F电容接GND,不用的输出可直接悬空
guanfu yuan 说:你好。我看了TVP7002的手册。我想知道的是该芯片能否将输入的模拟信号转换为6bit的数据输出。我不需要8bit的数据。是否我舍掉低两位就可以实现呢?还是需要设置。谢谢!
显示器是LVDS接口,就得需要DS90C363B这种将18bit RGB转换为LVDS接口的器件。guanfu yuan 说:你好,由于显示器是lvds(18bit)也就是需要将模拟vga信号转换为6bit的数字rgb信号!我想问一下tvp7002能实现么?谢谢!
你好!感谢您的解答。我这里还有一个问题就是如果采用TVP7002做设计的话。由于管教给的是10bit的。如果我输出RGB888的话。是否也是只需采用高8位就可以了。还有一个问题就是TVP7002IPZP 这种工业的片子还能买到么?我需要工业级的也就是工作温度在-20度。我看了这个片子的后缀,IPZP是工业级的。谢谢!