Other Parts Discussed in Thread: LMK04826
In the AFE58JD28EVM board, the OSCin input is 100MHz, the CLKin1 input is 125MHz, the DCLKout0 output is 200MHz, and VCO0 is selected in PLL2, how can VCO0 generate 2000MHz signal?
Because the range of VCO0 in the manual is 1840 to 1970MHz.