目前有个专案需用到SATA切换器,即将一组SATA1.0信号切换成两路,通过控制信号来选择哪一路通SATA1.0。在TI芯片里找到DS64MB201,比较符合要求。但具体运用上还有不明之处,该芯片具有输入Equalization和输出De-Emphasis。怎么才能关闭这两个功能,我只是用该芯片来进行SATA1.0信号切换。另外如下所示 Equalization Input设置等级时,三个档都是针对3GHz速率来讲,那我的信号是1.5GHz呢,是一样的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于速率,可以通过RATE引脚的高低电平来控制,或者直接悬空实现自动检测速率。
关于去加重和预加重的功能, 寄存器我看有EQ和DE的enable位。
但是如果你只是想实现SATA信号的切换,可以参考TS3DV642这款高速开关,不知电压符合不符合你的要求。
恩,如果采用ds64mb201,OOB信号能够支持,如果不需要Equalization功能,那么寄存器EQ control寄存器的bit[5:0]几位设置为100000,0x20 bypass。