This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298无法识别导联脱落问题求解答!很急,我在线等

Other Parts Discussed in Thread: ADS1298

你好!
       我是弈中医疗科技技术有限公司的工程师。
我用ADS1298实现了一个心电采集设备。发现无法通过读取寄存器的值来识别导联脱落。通过KEIL调试,读取配置后的寄存器的值,可以确定寄存器已有效进行了配置:LOFF=0X13;CONFIG4=0X02;LOFF_SENSP=LOFF_SENSN=0XFF(心电数据可以实时读取,但两个导联脱落状态的寄存器始终未0x00)。
      我配置的导联脱落检测方式是DC 电阻检测,按照手册说明的原理,当导联脱落后,差分通道的正端应该被上拉至AVDD(3.3V已测),但我测到的电压为290mV。我利用外部电阻392K强制将正端拉到AVDD,结果测量也只为2.3V,我用万用表测量引脚对地的电阻,是大于2M(我的万用表最大量程)的。不知道为什么?我测试了三个板子,都是一样的。现在我已将引脚外的滤波电路和防静电二极管都去掉了。