This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC63001: 关于DAC63001的电流输出

Part Number: DAC63001

您好,Ti,

我最近在设计一个电流源,是那种可编程的微功率直流电流源。我的直流输出范围在0~200uA觉得DAC63001芯片很适合我。

但是,我现在有几个问题,跟您请教:

1、DAC63001他的FB引脚,有什么用?我看了技术手册,技术手册上说,FBx引脚是用来做电压输出时候闭环使用。如果断开,就是比较器使用。请问,是这个意思么?如果我用DAC63001芯片做电流输出用,请问,我这个FBx引脚是否是需要断开,也就是float浮空使用??

2、DAC63001引脚,我做电流输出使用的时候,输出引脚Vout输出电流??那我问一句,此时Vout引脚的输出电压是什么?是否是技术手册P7页的表格数据Output??

3、我如何测量DAC63001芯片的输出的电流?我是否可以直接用6.5位万用表的直流电流档,一只表笔,直接接入到DAC63001芯片的Vout引脚,万用表另一端接芯片的GND上??是否需要在串接一直电阻进去??还是,串接电阻,我用6.5位万用表的直流电压档测量这个电阻的电压??

谢谢您,万分感谢您的帮助。