Other Parts Discussed in Thread: ADS8568
最近我在用ads8568发现一个奇怪的问题:在数据手册上写到其使用内部参考时,refio引脚输出电压默认情况下为2.5v,但是在实际测试中发现该引脚电平使用acdc供电时为2.5v,但当我将换成另外一个(暂时只试过朝阳的线性电源)为5v。电路设计采用手册推荐电阻电容。采用的硬件模式,内部参考电压。请问改参考电压还和其他有关么?This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS8568
最近我在用ads8568发现一个奇怪的问题:在数据手册上写到其使用内部参考时,refio引脚输出电压默认情况下为2.5v,但是在实际测试中发现该引脚电平使用acdc供电时为2.5v,但当我将换成另外一个(暂时只试过朝阳的线性电源)为5v。电路设计采用手册推荐电阻电容。采用的硬件模式,内部参考电压。请问改参考电压还和其他有关么?Hi ,
你所说的这种现象有几片是这样,还是仅有一片。正常应该是2.5V,如果出现你所说的情况,建议考虑是否芯片已经损坏。
使用内部参考,首先需要先将内部参考enable,可以采用硬件方式也可以采用软件方式,所以测试5V的时候,先检查下是否将内部参考enable。
REFIO为2.5V或3.0V都正常。