This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8568: 继电器动作导致ADS8568复位

Part Number: ADS8568


我的测试系统中,有三片ADS8568,用STM32单片机作为控制中心。系统初始化时,我配置它们的BUSY/INT引脚为低电平有效。系统还通过控制继电器动作实现电机的正反转,继电器触点开断的是AC 220V。当继电器不动作时,三片ADS8568工作正常。但是,当继电器动作时,经常出现ADS8568意外复位的现象(因为程序检测到BUSY/INT引脚的状态不对,在空闲时为低电平,也就是回到了芯片复位后的默认设置,而当这种意外发生时,重新配置ADS8568可以使ADS8568恢复正常)。整体来看,继电器动作导致ADS8568复位的概率在40%左右。请问这种现象的原因是什么?如何解决?