This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用DAC7568芯片作为C8051F系列单片机的DAC扩展芯片,参考连接图如下,想知道TXD和SCLK之间的元器件是反向放大器吗?要求什么型号,具体连接图是什么样子的呢?
另外,当参考电压是外接+5V时,VOUT的输出范围是0~5V吗?在VOUT端口接放大器OPA703(如下图)的目的是为了实现双极输出,若只需要输出0~5V电压,是不是就可以将VOUT直接接外部负载了?
普通反相器而已, 74HC00, CD40106 等等都能使用.
若只需要输出0~5V电压,是不是就可以将VOUT直接接外部负载了? 还是可能有问题, 原因是驱动能力不够. 当然这个芯片的输出最大短路电流达 11mA. 但不能用这个电流来衡量, 因为要保证精度, 负载还是尽量轻一点.
谢谢!另有一问题还请指教,DAC7568芯片与C8051之间的接线如图:但是由于MCU采用的是C8051F040芯片,其只有两组“TX RX”串行通信接口,均用于他用了,那么与DAC7568通讯的“TX RX”是否可采用普通I/O呢?若采用普通I/O的话程序的编写是否更加复杂?