Other Parts Discussed in Thread: LMX2581, TIDA-00360
我想测量gis的局部放电uhf,频率范围400到1500MHZ,请问这个TIDA-00360的作用是降频然后进行ad转换么,可以实现我的功能吗。如果可以,那么TIDA-00360是将400到1500Mhz降频,那LMX2581
- 输出频率:50MHz 至 3760MHz又有什么作用呢?初学者求指导
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMX2581, TIDA-00360
我想测量gis的局部放电uhf,频率范围400到1500MHZ,请问这个TIDA-00360的作用是降频然后进行ad转换么,可以实现我的功能吗。如果可以,那么TIDA-00360是将400到1500Mhz降频,那LMX2581
您好,
TIDA00360中的设计是下变频后进行AD转换。
但里面用到的ADC是16bit,370MSPS,应该是有美国出口管制的,需要License申请才能出售。
这个设计的信号带宽100M,也就是从400M到1500M中的任意100M带宽的信号下变频后进行AD采样。
Michael