是这样的,我采用了一片ADS1271,模式为高速SPI模式,我是采用上位机发送一个命令就采集1024个电压值,有一个问题就是每次采集的前面39值都是上次采集留下来的,例如我第一次ADC测量的是1V,那采样出来就是1024个1,如果我第二次把电压改为2v,采集的数据就变成了1,1,1,1,1,1,1,,,,(39个)...2.2.2.2.2.2.2.
看起来就想是ADC有记忆功能似的,例如我第三次把电压改为3V,采集的数据就变成了2,2,2,2,2,....(39个),......33333.我想问一下,这是为啥?