This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教关于选购AD和DA评估板的问题(接上一个问题)

1.选定满足指标(双通道,位数:12位;采样率:150MSPS)的AD和DA芯片评估板,要求所选定的AD和DA评估板可以配套使用。

2.选定AD和DA评估板,分别给出以下内容:

① AD和DA评估板型号和所在官网链接

② 评估板的官方价格(不是在淘宝上的,是官网上的)

③ 评估板的接口特性,即对于AD评估板,指出它是如何将数字信号传给PC的;对于DA评估板,指出它是如何与PC端口连接的。给出文档原文内容。

上面这个问题已经回答了,根据建议,我看了一下:AD的可以是ADS4126, DA的可以是DAC3161

这里还有两个问题:

(1)如果直接在官网上购买这两个评估板的话,这两个评估板是包括了所有套件吗?即买回来之后就可以直接用的,比如对于ADS4126这个评估板,买回来之后给定一个模拟信号就可以了,然后通过这个评估板就可以输出数字信号,再通过LVDS或CMOS给PC,是这样的吗?

(2)“ADS4126可以配置成LVDS或CMOS输出,DAC3161是LVDS输入。”这个具体是通过什么与PC连接了?