Part Number: ADC32J23
Other Parts Discussed in Thread: LMK04828
您好,我想询问能否使用HMC7043的
LVDS MODE (HIGH POWER)2模式实现对ADC32J23的SYSREF调制
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果ADI时钟器件的sysref电平足以满足ADC的需求,那么可以使用。我们不会回答有关竞争对手时钟设备技术细节的问题。
ADC接受0.9V的共模电压,即使与我们的LMK04828接口也需要非标准配置,即不是LVDS或LVPECL2000,而是LCPECL,在ADC引脚的100 ohm端接电阻之前需要一个7.5ohm的串联电阻。有关该配置的更多问题,请参考LMK04828。使用LCPECL与LMK04828接口时,请参考下面的原理图。