This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC80输出模拟电压错误

用DAC80-CBI-V数模转换芯片进行搭电路实验,希望产生-5V~+5V模拟电压输出,按说明书中"FUNCTIONAL DIAGRAM AND PIN ASSIGNMENTS"标题的典型电路搭建而成,其中输出引脚15连接引脚18,引脚16连接引脚24,引脚17连接引脚20,19引脚悬空,电源采用+-12V。无论输入端二进制输入数据如何变化,模拟信号输出端始终输出-5V,在试验中,将15脚连接到19脚后,正常输出-2.5V;将17脚与20脚断开后,测量20脚电压值为0V,不断开17脚与20脚,20脚电压仍然很小(0.001左右)。在试验中,通过电位器改变10K~100K处的阻抗,结果仍然如此。

      按此实验,本人猜测是否是数字转模拟的电阻网络出现问题?判定数字转模拟的电阻网络出问题依据是测17脚电压一直为0或很小。

      1.希望提供一个测试检测方案,是否是该芯片已损坏?在试验中用两块芯片,结果依然如此。

      2.如何得知数字转模拟电路部分出现问题?

      2.在调试中,我的方法是否有遗漏疏忽地方,请指出

                                                                                                                                                   ——谢谢