This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1262: 不确定读取的ADC内部温度传感器的数据是否正确?

Part Number: ADS1262


目的是读取ADS1262芯片的内部温度,使用内置的温度传感器;

参考数据手册进行了代码配置和操作:

寄存器配置如下:

POWER寄存器:0x13

INTERFACE寄存器:0x04

MODE0寄存器:0x00

MODE1寄存器:0x01

MODE2寄存器:0x08

INPMUX寄存器:0xBB

REFMUX寄存器:0x00

尝试读取了Analog power supply monitor和Digital power supply monitor,出来的数据都是对的;

但是读取温度传感器数据时,办公室开空调环境,裸板,电压是0.141V左右,按照公式计算实际温度是71度左右,但是手触摸芯片,肯定没有这么高,感觉40到50度之间吧;

板子冷启动后,温度传感器的温度确实会慢慢上升,最后保持在71度左右。

所以现在不确定问题出在什么地方?请帮忙解决。