Part Number: ADS1119
我使用ADS1119对3.6V的AC进行采样的时候,读出值是0X000000.
When I use the ADS1119 to sample a 3.6V AC signal, the readout value is 0X000000.
随后,我调整信号发生器的参数,此时电路的电压发生突变(示波器通道设置为直流(DC),从示波器中观察到的现象为峰值电压在7V左右),ADS1119此时的读出值为0xFFFFFF,在电路稳定后(示波器通道设置为直流(DC),从示波器中观察到的现象为偏置电压约为1V,峰峰值为3.6V的50Hz的正弦波),ADS1119的读出值又变为0x000000。
Subsequently, I adjusted the parameters of the signal generator, at which point the voltage in the circuit 突变 (the oscilloscope channel was set to DC, and the phenomenon observed on the oscilloscope was that the peak voltage was around 7V). The readout value of the ADS1119 at this time was 0xFFFFFF. After the circuit stabilized (the oscilloscope channel was set to DC, and the phenomenon observed on the oscilloscope was a 50Hz sine wave with an offset voltage of approximately 1V and a peak-to-peak value of 3.6V), the readout value of the ADS1119 changed back to 0x000000.
下面是该ADC的外围电路原理图。
Here is the schematic diagram of the peripheral circuit for this ADC.
VCC=3.3V。
AOUT1与采样的AC信号相连。
AOUT1 is connected to the AC signal being sampled.