Part Number: DAC61416
Other Parts Discussed in Thread: DAC81416
供电电压是41.6V,配置为0-40的范围,问题是最大输出到不了40V,只能到39.65V附近,问题可能出在哪里?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以对照参考下评估板的回路图和layout:
在0-40跨度内,最大输出仅为39.65。
请在下面提供详细信息以帮助您调试此问题-
1. REFIO引脚电压输出启用内部基准后,使用精度大于0.1mV的DDM进行测量
2. VSS,VCC和DAC81416引脚附近其它电源的值。
3.关于DAC VOUT负载的详细信息,如果有的话