This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC60704: Zero-scale error疑惑

Part Number: AMC60704

你好,在VDAC指标中有这样一项:Zero-scale error,在positive range时我理解,因为VSS最低就是0,VDAC输出被限制在0V以上,Zero-scale error只能往正偏。为什么在negative时只有负值呢?当code=0时,输出可以大于-5V呀,因为VSS最低可以-5.5V,是我理解错了吗?

  • 已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • negative ranges中,0实际上表示负满量程值。当DAC输出本应为0V时,就会出现这种错误。正负两个范围在偏离0V的最坏情况下误差相同,均为18mV。正范围为+18mV,负范围为-18mV。在负范围内,VCC(电源电压)为0V,这被视为零量程。在任何范围内,DAC输出都不可能等于电源轨电压。
    code 0的负向范围内,输出电压为-2.5V或-5V,具体取决于使用的增益设置。但上述规格指的是0V时的误差,而非code=0时的误差。