This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lmh0030 16bit数据输入 SDI输出



使用lmh0030将16bits数据转化为SDI输出,16bit分别用的是DV2-9和DV12-19,

现在是16bit有数据输入,但是SDI无输出,请问这是怎么回事?

只是将并行数据转化为串行数据时,lmh0030需要怎么配置?lmh0030的RD/WR引脚、ANC/CTRL引脚、ACLK引脚、AD引脚及IO引脚需不需要配置,

需要配置的话,该怎么配置?

之前我使用,只是将ANC/CTRL引脚拉高,其他引脚都悬空,16bit数据输入,SDI端有输出,但是之后不知怎么又没有输出了,这是怎么回事?

lmh0030该怎么配置?