This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: About unused pin

Part Number: ADS1299

As illustrated in the datasheet, I need to leave the NC(PIN27 29) and RESERVED(PIN64) open circuit, but the PDK connect the RESERVED PIN to AGND. I want to make sure which one is the best. And I am going to use ADS1299-4 ,should I connect the unused pin like IN8P and IN8N to the AVDD directly?