This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1263: 关于ADS1263使用外部基准的问题

Part Number: ADS1263

您好,我想问下我在使用外部基准电压芯片REF5050给ADS1263提供5V外部基准时 使用AIN2和AIN3作为外部输入的正负极  后续使用AIN0和AIN1作为差分输入端测量电压源电压时发现没有问题 但是当我去测量另外电路中某个电阻两端电压时 发现有极其严重的干扰 从AIN0和AIN1端会有漏电流输出!!十分确定漏电流来自REF5050, 因为使用内部基准时没有这种干扰。我现在的接线是REF5050的VOUT接AIN2 REF5050的GND接AIN3 这个接法存在问题吗?要怎么避免这种干扰呢?