This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS127L18: ADS127L18芯片上电测试电压CAPA-AVSS出现数据一直不稳定递减是为什么?

Part Number: ADS127L18

做的测试板芯片一上电就出现CAPA-AVSS电压从1.3V左右开始递减,会一直递减到接近不稳定的数据反复跳变,这是正常的吗?还是什么原因引起的?

  • 已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 这不是正常行为,电路板有问题(CAPA和AVSS之间的泄漏路径或接地),或者ADC或CAPA电容器有问题。

    问题:

    1.这是ADS127L18EVM-PDK主板还是客户主板?

    2.如果是客户板,使用的电容器值和部件号是什么? 指定值为10uF;低于4.7uF会导致稳定性问题。 此外,电容器的额定电压应至少为6V,以确保在直流偏置下,1.3V时的10uF电容器的电容大于4.7uF。