AFE5832LPEVM: AFE5832LPEVM: When using the swroop board, the Tx7332 transmission waveform cannot be acquired.

Part Number: AFE5832LPEVM
Other Parts Discussed in Thread: TX7332

Hi,

We are currently using the Swroop board to transmit multi-channel signals. When following the testing steps outlined in the Swroop user manual, we can observe the “Sync signal,” but we are unable to observe the output waveform from the Tx7332 (i.e., the “Tx7332 Output” shown in the diagram).

image.png

According to the manual, the +5V current limit is set to 1.5A and the -5V current limit is set to 200mA. After powering the board, the power supply displays as shown in the figure below. Is this correct?
image.png
Furthermore, after programming the FPGA bitfile, the voltage dropped from 5V to 3.3V, as shown in the figure below.

image.png

Is this normal? Could the chip have been burned out?

We look forward to your response!

Rachel