Other Parts Discussed in Thread: AMC1306M25, ADS1202
AMC1306M25的数据输出是1bit的,然后没有valid的信号,那么也就是我给clock,立马1bit数据出来(下降沿),我的问题是:
1,没有valid信号,怎么知道哪些数据流是有效的?
2,没有valid信号,怎么去判断数据流中,哪些bit组成一个16bit的数据?
3,可以用FPGA来接受数据吗?
AMC1306M25的数据输出是1bit的,然后没有valid的信号,那么也就是我给clock,立马1bit数据出来(下降沿),我的问题是:
1,没有valid信号,怎么知道哪些数据流是有效的?
2,没有valid信号,怎么去判断数据流中,哪些bit组成一个16bit的数据?
3,可以用FPGA来接受数据吗?
You can't just take 16-bits of data from the modulator and call it a day. All streams are valid and their filtered results reflect whatever is applied to the inputs. I'll try to find an app note or two that points out the high level detail of the inner working of a Delta Sigma Filter Module, but right now I can't think of any that go down to the bit-stream level.
You need to apply a digital filter to the output bit-stream in order to recover the original analog input waveform. That involves an over-sampling ratio and averaging the density of one's and zeros coming from the modulator. The decimation is what provides the 16-bit result, not just some random collection of this or that 16-bit stream.
Yes - a digital filter can be implemented in an FPGA, please refer to the code we published for the ADS1202 a while back.