我现在做4~20mA电流输出。想用DAC8750芯片实现。在看DAC8750的数据手册,发现并没有写DAC8750最低供电范围,只写有“最大环路依从电压: AVDD - 2V“,是不是可以这么理解,假如我用AVDD = 9V,负载RL最大的电压为 9 - 2 = 7V,也就是说,最大带载能力为 7V / 20mA = 350Ω;如果我需要带载250Ω,DAC8750最小AVDD = 250Ω * 20mA + 2 = 7V(理想状态下,不考虑线阻等)?
谢谢了。
”
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我现在做4~20mA电流输出。想用DAC8750芯片实现。在看DAC8750的数据手册,发现并没有写DAC8750最低供电范围,只写有“最大环路依从电压: AVDD - 2V“,是不是可以这么理解,假如我用AVDD = 9V,负载RL最大的电压为 9 - 2 = 7V,也就是说,最大带载能力为 7V / 20mA = 350Ω;如果我需要带载250Ω,DAC8750最小AVDD = 250Ω * 20mA + 2 = 7V(理想状态下,不考虑线阻等)?
谢谢了。
”
您好,不能小于10V的,AVDD-2都是在电源电压在10-36V之间的前提下的。
不仅仅使用DAC8750.使用其他芯片时也建议按照datasheet中推荐的电气参数使用,使得芯片达到最佳性能。