ADS1298ECGFE-PDK: How to check ADS1298ECGFE-PDK is still working?

Part Number: ADS1298ECGFE-PDK
Other Parts Discussed in Thread: ADS1294, ADS1298,

Hi, I have this ADS1298 which I bought last march. I know it is a lot past the return stage. But I have barely used the board and it started misbehaving. This started after I removed the MMB0 and used the ADS1298 with another microcontroller. ADS1298 was not giving any output after I connected it with nRF52833. I thought it was an issue because of serial communication. But when I connected it back to MMB0 board, I can't acquire data anymore. The SPS suddenly increased from 500 to 16000. And data acquisition failed. The TI software detects the board as ADS1294 instead of ADS1298. Then I followed a previously asked question-answer from the TI forum, which was shared to me. I updated the driver and SPS is now 500. But the board is not recognized by the software and it's written reset the hardware. I pressed reset and still nothing is happening. Please help.