Part Number: ADS127L11
Hi Team,
We are implementing your 24bit ADC ADS127L11IPWR in one of our design we need some clarification based on the datasheet.
We are providing AVDD +Ve voltage and AVSS -Ve voltage.
as per datasheet section 8.3.6.1 AVDD1 and AVSS For CAPA, AVDD1 & AVDD2 pins it is recommended to use the bypass capacitor (decap) to AVSS pin

In our application AVSS pin is connected to -ve voltage source. providing decaps to this source may couple noise to this source voltage.
We have referred your application circuit where -Ve voltage is not generated (AVSS was shorted with DGND with 0ohm; AVSS=0V). Hence decaps are provided to AVSS net which is AGND.
our query is
How decaps should be provided for our application (AVSS=-Ve voltage)?
shall we connect the decaps commonly to AGND for both AVDD and AVSS pins. (where AGND=0V)