AFE5832EVM: USE SPI CONTROL AFE5832EVM

Part Number: AFE5832EVM

you write  I need remove R140 if we use SPI control AFE5832EVM,but U14 and U13 enabled when  I remove R140,should I connect U14-PIN10 to GND for diabling U14 and U13.I am afraid if I dont do this,the SPI signal maybe bad.

  • 您好

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 我想用FPGA控制AFE5832EVM,你们的用户手册里面说只用把U14芯片旁边的R140拆除了就可以用外部SPI控制了,按照我的想法如果拆除了R140,那么USB应该就不能用了,也就是不使能了,但是现在的情况是,U14仍然是使能,也就是说他还是会输出高电平也就是3V3,它还是一个强上拉输出,可能会跟我的FPGA输出的SPI冲突到一块,导致信号失真甚至烧毁板子,这是我的理解看您那边是怎么处理的。

  • 您好

    Yes, you can connect Pin10 to ground to disable the SPI control through the USB.