This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8734: DAC8734驱动LM4755的连接问题。

Part Number: DAC8734
Other Parts Discussed in Thread: LM4755,

您好,我的项目使用DAC8734驱动4通道LM4755,单端驱动模式,LM4755采用独立的±24V供电。LM4755的layout遵循说明书建议,输出和输入部分采用独立的地环路。DAC8734单端输出,经过低通滤波,通过4对信号和地的信号对分别连接4个LM4775输入引脚和接地引脚。当LM4755工作后,遇到如下问题

1 DAC部分噪声明显增加,那么DAC应当以什么方式驱动LM4755,减少高功率部分对精密部分的影响?是否有参考设计。

2 4个LM4755之间串扰明显。多片LM4755在一个板子,共享一个端子供电情况下,单点接地位置应如何选择?如何降低通道串扰?如何与DAC连接?