This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1248EVM-PDK: ADS1248评估板断电模式与功耗异常问题

Part Number: ADS1248EVM-PDK
Other Parts Discussed in Thread: ADS1248

我正在评估ADS1248的性能指标,遇到了一些问题需要您的帮助。

  1. 测试电源项目断电模式功耗:当START引脚处于低电平时,所有寄存器值被复位为0。此时无法进行数据采样(内部时钟可能被关闭),内部REF可能被关断,且无法再进行SPI通信。断电模式下是否就是这种情况?备注:IDVDD电流是移除R6电阻后,在R6位置串入七位半电流表进行测试的,因为IDVDD电流较小,因此,并未使用欧姆法进行测试。
  2. 正常工作状态下,DVDD = AVDD = 5V,数据速率DR = 20 SPS,使用内部振荡器,外部参考电压。实测IDVDD电流为1223.7uA,明显高于数据手册标称的230uA。测试时AIN0至AIN7的VIBAS电压设置为AVDD/2,SCLK、DIN和DOUT均设为低电平,且移除了电阻R17和R18。在DVDD=AVDD=5V的条件下,还有哪些因素可能导致IDVDD电流异常?也实验了另外一种情况,把AINP、AINN设置为VBIAS电压时,或模拟输入均不连接到VIBAS电压时,电流仍然较大。
  3. 在测试内部和外部振荡器的工作电流时,发现使用外部时钟时的IDVDD电流比使用内部振荡器时高出约30微安。这种情况是否合理?造成这种电流差异的可能原因有哪些?数据手册中提到外部时钟工作时会停用内部振荡器,此时IDVDD不是应该更小吗?