你好,我在贵公司官网有看到一颗芯片DS100DF410,我们想做一款20米DP的延长线驱动,不知该芯片是否合适?如可以贵公司是否有应用的实例,比如外部EEPROM的配置等,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我在贵公司官网有看到一颗芯片DS100DF410,我们想做一款20米DP的延长线驱动,不知该芯片是否合适?如可以贵公司是否有应用的实例,比如外部EEPROM的配置等,谢谢。
这是一个10G的retimer。用来进行数据调理的。加重,均衡等
EEPROM可以从网上下载EVM的软件,免费,他会按照你的要求生成EEPROM
OK,另外贵公司的SN65DP140是不是不会量产,如果是的话TI替代这颗物料是那一颗,我有找到SNDP130这颗芯片,可是该芯片的VOD功能只能是通过link training或者I2C来配置,这样一来就没有GPIO配置这个功能了(我们需要级联),是这样的吗?
TI网上已经没有SN65DP140的资料了,根据您的要求,可以考虑SN65DP141,可以使用GPIO或I2C两种配置方式。
Kailyn Chen:
你好,不知道TI中国是哪一位FAE专职负责SN65DPxxx和SN75DPxxx系列芯片,烦请告知他的联系方式,我有些细节想与他们沟通,谢谢。
可以联系下当地授权代理商的FAE:
http://www.ti.com.cn/general/cn/docs/gencontent.tsp?contentId=24957