Part Number: ADS8556
1、当前ADS8556 HVDD采用+5.2V供电,HVSS采用-5.2V供电,芯片对HVDD和HVSS上下电时序有要求吗?如果有规格是怎样的?会否导致假设HVDD先上电导致HVSS被拉至正电压?
2、ADS8556对HVDD和HVSS上电斜率、下电斜率有要求吗?如果有规格是怎样的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS8556
1、当前ADS8556 HVDD采用+5.2V供电,HVSS采用-5.2V供电,芯片对HVDD和HVSS上下电时序有要求吗?如果有规格是怎样的?会否导致假设HVDD先上电导致HVSS被拉至正电压?
2、ADS8556对HVDD和HVSS上电斜率、下电斜率有要求吗?如果有规格是怎样的?
需要进一步确认:
1.假设正电压HVDD(5.2V)比 HVSS(-5.2V)先上会不会导致HVSS拉高超过到0.3V以上?反之,正电压HVSS(-5.2V)比 HVDD(+5.2V)先上会不会导致HVSS拉高超过到-0.3V以下?
2.HVDD采用5.2V供电,HVSS采用-5.2V供电是否可靠无风险?(采用内部REF 2.5V,输入模拟量-5.2V-5.2V)
3.如果HVDD有瞬时(ms)小于-0.3V:HVSS瞬时(ms)大于0.3V有什么风险?是如何评估出来的?
以上,期待回复,感谢