This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE58JD48: AFE58JD48在JESD204B 40X模式下使用Demod功能建链异常

Part Number: AFE58JD48
Other Parts Discussed in Thread: AFE58JD32

一、参考手册:当前设计时所使用的参考手册为《AFE58JD48 (SBAS881A –OCTOBER 2019–REVISED DECEMBER 2019).PDF》

二、故障描述:

1)采用125Mhz的系统时钟,JESD204B配置参数为L=4,PLL模式为40X,K=8,S=1,M=8。

未启用Demod功能的情况下,AFE58JD32功能均正常。

启用Demod功能后(同时启用DEC功能与DWN_CNV功能),且配置0x9c寄存器当中的MANUAL_DECIMATION_FACTOR参数为2,COMPR_ FACTOR为0,JESD204B无法建链。但手册当中的表64有对该用法有阐述说明,似乎支持此类用法。

启用Demod功能后(同时启用DEC功能与DWN_CNV功能),且配置0x9c寄存器当中的MANUAL_DECIMATION_FACTOR参数为4,COMPR_ FACTOR为0,MANUAL_FSWEEP_START配置为0时,发送TX_TRIG信号后JESD204B功能正常,未掉链。当配置MANUAL_FSWEEP_START为非零值时,发送TX_TRIG信号后JESD204B会掉链,无法稳定通信。

2)采用125Mhz的系统时钟,JESD204B配置参数为L=2,PLL模式为40X,K=8,S=1,M=4。

启用Demod功能后(同时启用DEC功能与DWN_CNV功能),且配置0x9c寄存器当中的MANUAL_DECIMATION_FACTOR参数为2,COMPR_ FACTOR为1,MANUAL_FSWEEP_START配置为0时,发送TX_TRIG信号后JESD204B功能正常。当配置MANUAL_FSWEEP_START为非零值时,发送TX_TRIG信号后JESD204B会掉链,依然无法稳定通信。

其他抽取比例类似情况。

3)本人也尝试过JESD204B与DEMOD的多种组合手段,均未有显著变化。

三、需要获取的帮助

1)能否提供一份较为完整的在启用DEMOD全部功能的情况下,40X模式的JESD204B版本的Demod功能完整寄存器配置流程?如2倍或4倍抽取的操作案例。

2)能否确认开发手册是否为最新的,因为在手册当中有部分功能比较模糊,如介绍40X模式时,特意强调了在启用Demod功能且在2倍抽取的情况下,需要修改JESD204B的L与M参数。但DWN_CNW会输出16相位,FS/2的数据流,此时Demod的带宽和不启用Demod时应该保持一致的,除非是DWN_CNV被关闭。