This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS8200 VGA_HS_OUT时钟不稳定的问题?

Other Parts Discussed in Thread: THS8200, THS7303

最近在调试THS8200芯片,VGA显示720P分辨率的时候,图像会有水平的重影,用示波器量61管脚HS_OUT,发现HS_OUT不稳,请问应该调那些寄存器解决。

  • 你好,你的问题应该顺利解决了吧。

    现在我自己在着手配置VGA输出,遇到了不少困难,很不成功。在这里向你请教。

    后面是dm6467与ths8200的连接示意图,。我没有用cde,用的是固定晶振。

     1,DM6467输出BT1120,那么VPIF_CLKIN2必须输入74.25M作为BT1120的同步频率,这个认识是否正确?

    2,个人认为VPIF_CLKOUT2与VPIF_CLKIN2是一样的,是否是这样,如果不是如何配置VPIF_CLKOUT2?

    3,如果1,2是肯定的,那么VPIF_CLKOUT2输出也是为74.25M,但是SXGA1400X1050需要105M的时钟,这就无法实现了。所以个人认为1,2肯定有一个错。但是无法肯定。

     4,ths8200的输出应该与vpif无关,就是说我要得到VGA输出只要配置ths8200的寄存器就行了,不需要做另外的更改,ths7303也不要更改,是否是这样? 望不吝赐教,十分感谢!